13.33.179 smartpower_set_preferences
smartpower_set_preferences -powerunit {value} -frequnit {value} -opmode {value} -opcond
{value} -toggle {value}
Sets the following preferences: power unit, frequency unit, operating mode, operating conditions, and toggle. These preferences can also be set from the preferences dialog box.
Arguments
-powerunit {value}
Specifies the unit in which power is set. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
W |
The power unit is set to watts |
|
mW |
The power unit is set to milliwatts |
|
uW |
The power unit is set to microwatts |
-frequnit {value}
Specifies the unit in which frequency is set. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
Hz |
The frequency unit is set to hertz |
|
kHz |
The frequency unit is set to kilohertz |
|
MHz |
The frequency unit is set to megahertz |
-opmode {value}
Specifies the operating mode. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
active |
The operating mode is set to active |
|
static |
The operating mode is set to static |
|
sleep |
The operating mode is set to sleep |
|
Flash*Freeze |
The operating mode is set to Flash*Freeze |
|
shutdown |
The operating mode is set to shutdown |
-opcond {value}
| Value | Description |
|---|---|
|
worst |
The operating condition is set to worst case |
|
typical |
The operating condition is set to typical case |
|
best |
The operating condition is set to best case |
-toggle {value}
Specifies the toggle. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
true |
The toggle is set to true |
|
false |
The toggle is set to false |