13.33.106 new_design

new_design -name design_name -family family_name –path pathname–block value

Creates a new design. You need all three arguments for this command. This command will set up the Designer software for importing design source files

Arguments

-name design_name

The name of the design. This is used as the base name for most of the files generated from Designer.

-family family_name

The Actel device family for which the design is being targeted.

-path path_name

The physical path of the directory in which the design files will be created.

block value

Enables or disables Block mode. The following table shows the acceptable values for this option:
ValueDescription

on

Enables Block mode

off

Disables Block mode