13.33.133 set_clock_uncertainty
set_clock_uncertainty uncertainty -from | -rise_from | -fall_from from_clock_list -to | - rise_to | -fall_to to_clock_list -setup {value} -hold {value}
Specifies a clock-to-clock uncertainty between two clocks (from and to) and returns the ID of the created constraint if the command succeeded.
Arguments
uncertainty
Specifies the time in nanoseconds that represents the amount of variation between two clock edges.
-from
Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the source clock list. Only one of the -from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
-rise_from
Specifies that the clock-to-clock uncertainty applies only to rising edges of the source clock list. Only one of the - from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
-fall_from
Specifies that the clock-to-clock uncertainty applies only to falling edges of the source clock list. Only one of the - from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
from_clock_list
Specifies the list of clock names as the uncertainty source.
-to
Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the destination clock list. Only one of the -to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
-rise_to
Specifies that the clock-to-clock uncertainty applies only to rising edges of the destination clock list. Only one of the
-to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
-fall_to
Specifies that the clock-to-clock uncertainty applies only to falling edges of the destination clock list. Only one of the -to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
to_clock_list
Specifies the list of clock names as the uncertainty destination.
-setup
Specifies that the uncertainty applies only to setup checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks.
-hold
Specifies that the uncertainty applies only to hold checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks.