13.33.190 st_edit_set
Modify the paths in a user set.
st_edit_set -name name
[-source pin_list ] [-sink pin_list ] [-rename_to name ]
Arguments
-name name
Specifies the name of the set to modify.
-source pin_list
If the set is a subset of another set, specifies a filter on the source pins from the parent set. Otherwise, this option specifies the source pins of the set.
-sink pin_list
If the set is a subset of another set, specifies a filter on the sink pins from the parent set. Otherwise, this option specifies the sink pins of the set.
-rename_to name
Specifies a new name for the set.