13.33.122 remove_input_delay
remove_input_delay -clock clock_name port_pin_list
remove_input_delay -id constraint_ID
Removes an input delay a clock on a port by specifying both the clocks and port names or the ID of the input_delay constraint to remove.
Arguments
-clock clock_name
Specifies the clock name to which the specified input delay value is assigned.
port_pin_list
Specifies the port names to which the specified input delay value is assigned.
-id constraint_ID
Specifies the ID of the clock with the input_delay value to remove from the current scenario. You must specify either both a clock name and list of port names or the input_delay constraint ID .