13.33.110 pin_fix

Locks the pin assignment for the specified port, so the pins cannot be moved during place-and-route.

pin_fix -port portname

Note: You can use this command for designs created with PinEditor in MVN and PinEditor (non-MVN).

Arguments

-port portname

Specifies the name of the port to which the pin must be locked at its assigned location.
Note: You can assign only one pin to a port.