13.33.174 smartpower_set_cooling

Sets the cooling style to one of the predefined types, or a custom value.

smartpower_set_cooling -style {value} -teta {value}

Arguments

-style {value}

Specifies the cooling style to custom value or to one of the predefined types with a default thermal resistance value. The following table shows the acceptable values for this argument:

ValueDescription

300_lfm

Predefined cooling style

case_cooling

Predefined cooling style

still_air

Predefined cooling style

custom

Cooling style defined by user input

-teta {value}

Specifies the thermal resistance in °C/W. This argument is only available when style is set to Custom.