13.33.138 set_disable_timing
Disables timing arcs within a cell and returns the ID of the created constraint if the command succeeded.
set_disable_timing -from value -to value name
Arguments
-from from_port
Specifies the starting port. The –from and –to arguments must either both be present or both omitted for the constraint to be valid.
-to to_port
Specifies the ending port. The –from and –to arguments must either both be present or both omitted for the constraint to be valid.
name
Specifies the cell name where the timing arcs will be disabled.