13.33.132 set_clock_latency
puts “Design saved successfully” # Proceed to make further changes
Defines the delay between an external clock source and the definition pin of a clock within SmartTime.
set_clock_latency -source [-rise][-fall][-early][-late] delay clock
Arguments
-source
Specifies the source latency on a clock pin, potentially only on certain edges of the clock.
-rise
Specifies the edge for which this constraint will apply. If neither or both rise are passed, the same latency is applied to both edges.
-fall
Specifies the edge for which this constraint will apply. If neither or both rise are passed, the same latency is applied to both edges.
-invert
Specifies that the generated clock waveform is inverted with respect to the reference clock.
-late
Optional. Specifies that the latency is late bound on the latency. The appropriate bound is used to provide the most pessimistic timing scenario. However, if the value of "-late" is less than the value of "-early", optimistic timing takes place which could result in incorrect analysis. If neither or both "-early" and "-late" are provided, the same latency is used for both bounds, which results in the latency having no effect for single clock domain setup and hold checks.
-early
Optional. Specifies that the latency is early bound on the latency. The appropriate bound is used to provide the most pessimistic timing scenario. However, if the value of "-late" is less than the value of "-early", optimistic timing takes place which could result in incorrect analysis. If neither or both "-early" and "-late" are provided, the same latency is used for both bounds, which results in the latency having no effect for single clock domain setup and hold checks.
delay
Specifies the latency value for the constraint.
clock
Specifies the clock to which the constraint is applied. This clock must be constrained.