13.33.119 remove_disable_timing
remove_disable_timing -from value -to value name -id name
Removes a disable timing constraint by specifying its arguments, or its ID. If the arguments do not match a disable timing constraint, or if the ID does not refer to a disable timing constraint, the command fails.
Arguments
-from from_port
Specifies the starting port. The –from and –to arguments must either both be present or both omitted for the constraint to be valid.
-to to_port
Specifies the ending port. The –from and –to arguments must either both be present or both omitted for the constraint to be valid.
name
Specifies the cell name where the disable timing constraint will be removed. It is an error to supply both a cell name and a constraint ID, as they are mutually exclusive. No wildcards are allowed when specifying a clock name, either alone or in an accessor command1.
-id name
Specifies the constraint name where the disable timing constraint will be removed. It is an error to supply both a cell name and a constraint ID, as they are mutually exclusive. No wildcards are allowed when specifying a clock name, either alone or in an accessor command1.