13.33.25 organize_sources
Organizes the source files in your project.
-organize_sources
[-file name]*
[-mode value]
-module value
-tool value
[-use_default value]Arguments
-file name
Specifies the name of the file to which you want to associate your stimulus files.
-mode value
Specifies whether you are creating a new stimulus association, adding, or removing; possible
values are:
| Value | Description |
|---|---|
|
new |
Creates a new stimulus file association |
|
add |
Adds a stimulus file to an existing association |
|
remove |
Removes an stimulus file association |
-module value
Sets the module, where value is the name of the module.
-tool value
Identifies the intended use for the file, possible values are:
| Value | Description |
|---|---|
|
synthesis |
File to be used for synthesis |
|
simulation |
File to be used for simulation |
-use_default value
Uses the default values for synthesis or simulation; possible values are:
| Value | Description |
|---|---|
|
TRUE |
Uses default values for synthesis or simulation. |
|
FALSE |
Uses user-defined values for synthesis or simulation |