13.33.24 Arguments
organize_constraints
Organizes the constraint files in your project.
-organize_constraints
[-file name]*
[-mode value]
-designer_view name
-module value
-tool value-file name
Specifies the name of the file to which you want to associate your stimulus files.
-mode value
Specifies whether you are creating a new stimulus association, adding, or removing; possible values are:
| Value | Description |
|---|---|
|
new |
Creates a new stimulus file association |
|
add |
Adds a stimulus file to an existing association |
|
remove |
Removes an stimulus file association |
-designer_view name
Sets the name of the Designer View in which you wish to add the constraint file, where name is the name of the view (such as impl1).
-module value
Sets the module, where value is the name of the module.
-tool value
Identifies the intended use for the file, possible values are:
| Value | Description |
|---|---|
|
synthesis |
File to be used for synthesis |
|
designer |
File to be used in Designer |
|
phsynth |
File to be used in physical synthesis |