13.33.198 timer_add_stop
Adds the specified pin to the list of pins through which the paths will not be displayed in the timing analysis tool.
timer_add_stop -pin pin_name
Arguments
-pin pin_name
Specifies the name of the pin through which the path will not be displayed.