13.33.81 import_aux
Imports the specified auxiliary file into the design. Equivalent to executing the Import Auxiliary Files command from the File menu.
import_aux
-format file_type-partial_parse value
-start_time value
-end_time value
-auto_detect_top_level_name value
-top_level_name value
-glitch_filtering value
-glitch_threshold value
filename
Arguments
-format file_type
Specifies the file format of the file to import. You can import one of the following types of files: pdc, sdc, pin, dcf, saif, vcd, or crt.
-partial_parse {value}
Specifies whether to partially parse the *.vcd file. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Partially parses the *.vcd file |
false | Does not partially parse the *.vcd file |
-start_time {value}
This option is available only if -partially_parse is set to true. Specifies the start time (in ns) to partially parse the *.vcd file.
-end_time {value}
This option is available only if -partially_parse is set to true. Specifies the end time (in ns) to partially parse the *.vcd file.
-auto_detect_top_level_name {value}
Specifies whether to automatically detect the top-level name. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Automatically detects the top-level name |
false | Does not automatically detect the top-level name |
-top_level_name top_level_name
Specifies the instance name of your design in the simulation testbench when you import a VCD or SAIF file.
When importing a VCD file, the automatic top_level_name detection is available. If the -top_level_name option is not specified, SmartPower will try to automatically detect the top level name.
When importing a SAIF file, the automatic top_level_name detection is not available and -top_level_name is a required argument.
To identify the top_level_name for SAIF and VCD files manually, refer to Importing a VCD file and Importing a SAIF file.
-glitch_filtering {value}
Specifies whether to use glitch filtering. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
true | Glitch filtering is on |
auto | Enables automatic glitch filtering. This option will ignore any value specified in -glitch_threshold |
false | Glitch filtering is off |
-glitch_threshold {value}
This option is only available when -glitch_filtering is set to true. Specifies the glitch filtering value in ps.
filename
Specifies the name of the auxiliary file to import.