13.33.178 smartpower_set_pin_frequency
smartpower_set_pin_frequency -pin_name {pin_name} -pin_freq {value}
Sets the frequency of a pin in megahertz (MHz). If you do not use this command, each pin will have default frequency based on its domain.
Arguments
-pin_name {pin_name}
Specifies the name of the pin for which the frequency will be set.
-pin_freq {value}
Specifies the value of the frequency in MHz, which can be any positive decimal number.