13.33.185 smartpower_temperature_opcond_set_mode_specific
Sets the temperature for SmartPower mode-specific operating conditions.
smartpower_temperature_opcond_set_mode_specific -mode{value} -best{value} -typical{value} - worst{value} -thermal_mode{value}
Arguments
-mode{value}
Selects the mode to which apply the operating condition settings. You can select a pre-defined mode or any custom mode in your design.
-best{value}
Specifies the best temperature (in degrees Celsius) for the selected mode.
-typical{value}
Specifies the typical temperature (in degrees Celsius) for the selected mode.
-worst{value}
Specifies the worst temperature (in degrees Celsius) for the selected mode.
-thermal_mode{value}
Specifies the mode in which the junction temperature is computed. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
ambient |
The junction temperature will be iteratively computed with total static power |
|
opcond |
The junction temperature will be given as one of the operating condition range values specified in the device selection |