13.33.142 set_min_delay
Specifies the minimum delay for the timing paths in the current scenario.
set_min_delay delay_value [-from from_list] [-to to_list] [-through through_list]
Arguments
delay_value
Specifies a floating point number in nanoseconds that represents the required minimum delay value for specified paths.
- If the path starting point is on a sequential device, the tool includes clock skew in the computed delay.
-from from_list
- If the path starting point has an input delay specified, the tool adds that delay value to the path delay.
- If the path ending point is on a sequential device, the tool includes clock skew and library setup time in the computed delay.
- If the ending point has an output delay specified, the tool adds that delay to the path delay.
Specifies a list of timing path starting points. A valid timing starting point is a clock, a primary input, an inout port, or a clock pin of a sequential cell.
-to to_list
Specifies a list of timing path ending points. A valid timing ending point is a clock, a primary output, an inout port, or a data pin of a sequential cell.
-through through_list
Specifies a list of pins, ports, cells, or nets through which the timing paths must pass.