13.33.200 timer_get_path
Displays the path between the specified pins in the Log window.
timer_get_path -from source_pin -to destination_pin
[-exp value]\ [-sort value]\ [-order value]\ [-case value]\
[-maxpath maximum_paths]\
[-maxexpath maximum_paths_to_expand]\ [-mindelay minimum_delay]\
[-maxdelay maximum_delay]\ [-breakatclk value]\
[-breakatclr value]
Arguments
-from source_pin
Specifies the name of the source pin for the path.
-to destination_pin
Specifies the name of the destination pin for the path.
-exp value
Specifies whether to expand the path. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
yes |
Expands the path |
|
no |
Does not expand the path |
-sort value
Specifies whether to sort the path by either the actual delay or slack value. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
actual |
Sorts the path by the actual delay value |
|
slack |
Sorts the path by the slack value |
-order value
Specifies whether the list is based on maximum or minimum delay analysis. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
long |
The paths are listed based on the maximum delay analysis |
|
short |
The paths are listed based on the minimum delay analysis |
-case value
Specifies whether the report will include the worst, typical, or best case timing numbers. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
worst |
Includes worst case timing numbers |
|
typ |
Includes typical case timing numbers |
|
best |
Includes best case timing numbers |
-maxpath maximum_paths
Specifies the maximum number of paths to display.
-maxexpath maximum_paths_to_expand
Specifies the maximum number of paths to expand.
-mindelay minimum_delay
Specifies the path delay in the minimum delay analysis mode.
-maxdelay maximum_delay
Specifies the path delay in the maximum delay analysis mode.
-breakatclk value
Specifies whether to break the paths at the register clock pins. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
yes |
Breaks the paths at the register clock pins |
|
no |
Does not break the paths at the register clock pins |
-breakatclr value
Specifies whether to break the paths at the register clear pins. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
yes |
Breaks the paths at the register clear pins |
|
no |
Does not break the paths at the register clear pins |