13.33.52 About Designer Tcl Commands
A Tcl (Tool Command Language) file contains scripts for simple or complex tasks. You can run
scripts from either the Windows or UNIX command line or store and run a series of Tcl
commands in a “.tcl” batch file. You can also run scripts from within
Designer.
| Command | Action |
|---|---|
|
add_probe |
Adds a probe to an internal net in your design, using the original name from the optimized netlist in your design. Also, this command must be used in conjunction with the generate_probes command to generate a probed ADB file (see example below). |
|
all_inputs |
Returns an object representing all input and inout pins in the current design |
|
all_outputs |
Returns an object representing all output and inout pins in the current design |
|
all_registers |
Returns an object representing register pins or cells in the current scenario based on the given parameters |
|
are_all_source_files_current |
Audits all source files and determines whether or not they are out of date / imported into the workspace |
|
backannotate |
Extracts timing delays from your post layout data |
|
check_timing_constraints |
Checks all timing constraints in the current timing scenario for validity |
|
clone_scenario |
Creates a new timing scenario by duplicating an existing one |
|
close_design |
Closes the current design |
|
compile |
Performs design rule check and optimizes the input netlist before translating the source code into machine code |
|
create_clock |
Creates a clock constraint on the specified ports/pins, or a virtual clock if no source is specified |
|
create_generated_clock |
Creates an internally generated clock constraint on the ports/pins and defines its characteristics |
|
create_scenario |
Creates a new timing scenario with the specified name |
|
delete_probe |
Deletes a probe on nets in a probed ADB file |
|
delete_scenario |
Deletes the specified timing scenario |
|
export |
Converts a file from its current format into the specified file format, usually for use in another program |
|
extended_run_shell |
Runs multiple iterations of layout through Designer |
|
generate_probes |
Executes the probing and creates a new ADB file. This command is used in conjunction with the add_probe Tcl command (see example below). |
|
get_cells |
Returns an object representing the cells (instances) that match those specified in the pattern argument |
|
get_clocks |
Returns an object representing the clock(s) that match those specified in the pattern argument in the current timing scenario |
|
get_current_scenario |
Returns the name of the current timing scenario |
|
get_defvar |
Returns the value of the Designer internal variable you specify |
|
get_design_filename |
Returns the fully qualified path of the specified design file |
|
get_design_info |
Returns detailed information about your design, depending on which arguments you specify |
|
get_nets |
Returns an object representing the nets that match those specified in the pattern argument |
|
get_out_of_date_files |
Audits all files returns a list of filenames that are out of date |
|
get_pins |
Returns an object representing the pin(s) that match those specified in the pattern argument |
|
get_ports |
Returns an object representing the port(s) that match those specified in the pattern argument |
|
import_aux |
Imports the specified file as an auxiliary file, which are not audited and do not require you to re-compile the design |
|
import_source |
Imports the specified file as a source file, which include your netlist and design constraints |
|
ioadvisor_apply_suggestion |
Applies the suggestions for the selected attribute to the selected I/O(s) |
|
ioadvisor_commit |
Saves all changes in the I/O Advisor |
|
ioadvisor_restore |
Restores the I/O Advisor to the initial state |
|
ioadvisor_restore_initial_value |
Sets the current value for the selected attribute and I/Os to the initial value |
|
ioadvisor_set_outdrive |
Sets the outdrive for the selected I/Os |
|
ioadvisor_set_outputload |
Sets the output load for the selected I/Os |
|
ioadvisor_set_slew |
Sets the slew for the selected I/Os |
|
is_design_loaded |
Returns True if the design is loaded into Designer; otherwise, returns False |
|
is_design_modified |
Returns True if the design has been modified since it was last compiled; otherwise, returns False |
|
is_design_state_complete |
Returns True if the specified design state is complete (for example, you can inquire as to whether a die and package has been selected for the design); otherwise, returns False |
|
is_source_file_current |
Audits the source file and determines whether or not the file is out of date/imported into the workspace |
|
layout |
Place-and-route your design |
|
layout (advanced options for the SX family) |
Sets advanced place-and-route features for SX family designs |
|
layout - Axcelerator |
Sets advanced place-and-route features for Axcelerator family designs |
|
list_clocks |
Returns details about all of the clock constraints in the current timing constraint scenario |
|
list_clock_latencies |
Returns details about all of the clock latencies in the current timing constraint scenario |
|
list_clock_uncertainties |
Returns the list of clock-to-clock uncertainty constraints for the current scenario. |
|
list_disable_timings |
Returns the list of disable timing constraints for the current scenario |
|
list_false_paths |
Returns details about all of the false paths in the current timing constraint scenario |
|
list_generated_clocks |
Returns details about all of the generated clock constraints in the current timing constraint scenario |
|
list_input_delays |
Returns details about all of the input delay constraints in the current timing constraint scenario |
|
list_max_delays |
Returns details about all of the maximum delay constraints in the current timing constraint scenario |
|
list_min_delays |
Returns details about all of the minimum delay constraints in the current timing constraint scenario |
|
list_multicycle_paths |
Returns details about all of the multicycle paths in the current timing constraint scenario |
|
list_objects |
Returns a list of names of the objects in the specified list |
|
list_output_delays |
Returns details about all of the output delay constraints in the current timing constraint scenario |
|
list_scenarios |
Returns a list of names of all of the available timing scenarios |
|
new_design |
Creates a new design (.adb) file in a specific location for a particular design family such as Axcelerator or ProASIC3 |
|
open_design |
Opens an existing design in the Designer software |
|
pin_assign |
Assigns the named pin to the specified port but does not lock its assignment. |
|
pin_commit |
Saves the pin assignments to the design (.adb) file. |
|
pin_fix |
Locks the pin assignment for the specified port, so the pin cannot be moved during place-and-route. |
|
pin_fix_all |
Locks all the assigned pins on the device so they cannot be moved during place-and-route. |
|
pin_unassign |
Unassigns a specific pin from a specific port. The unassigned pin location is then available for other ports. |
|
pin_unassign_all |
Unassigns all pins from a specific port. |
|
pin_unfix |
Unlocks the specified pin from its port. |
|
layout (advanced options for ProASIC |
Sets advanced place-and-route features for ProASIC family designs |
|
remove_clock |
Removes the specified clock constraint from the current timing scenario |
|
remove_clock_latency |
Removes a clock source latency from the specified clock and from all edges of the clock |
|
remove_clock_uncertainty |
Removes a clock-to-clock uncertainty from the current timing scenario by specifying either its exact arguments or its ID |
|
remove_disable_timing |
Removes a disable timing constraint by specifying its arguments, or its ID |
|
remove_false_path |
Removes a false path from the current timing scenario by specifying either its exact arguments or its ID |
|
remove_generated_clock |
Removes the specified generated clock constraint from the current scenario |
|
remove_input_delay |
Removes an input delay a clock on a port by specifying both the clocks and port names or the ID of the input_delay constraint to remove |
|
remove_max_delay |
Removes a maximum delay constraint in the current timing scenario by specifying either its exact arguments or its ID. |
|
remove_min_delay |
Removes a minimum delay constraint in the current timing scenario by specifying either its exact arguments or its ID |
|
remove_multicycle_path |
Removes a multicycle path constraint in the current timing scenario by specifying either its exact arguments or its ID |
|
remove_output_delay |
Removes an ouput delay by specifying both the clocks and port names or the ID of the output_delay constraint to remove |
|
rename_scenario |
Renames the specified timing scenario with the new name provided |
|
report |
Generates the type of report you specify: Status, Timing, Timer Violations, Flip-flop, Power, Pin, or I/O Bank |
|
report (Activity and Hazards Power Report) |
Reads a VCD file and reports transitions and hazards for each clock cycle of the VCD file. |
|
report (Bottleneck) using SmartTime |
Creates a bottleneck report |
|
report (Cycle Accurate Power Report) |
Reports a power waveform with one power value per clock period or half-period instead of an average power for the whole simulation |
|
Report (Data History) |
Reports new features and enhancements, bug fixes and known issues for the current release that may impact the power consumption of the design |
|
report (Datasheet) using SmartTime |
Creates a datasheet report |
|
Report (Power) |
Creates a Power report, which enables you to determine if you have any power consumption problems in your design |
|
Report (Power Scenario) |
Creates a scenario power report, which enables you to enter a duration for a sequence of previously defined power modes and calculate the average power consumption and the excepted battery life for this sequence. |
|
report (Timing) using SmartTime |
Creates a timing report |
|
report (Timing violations) using SmartTime |
Creates a timing violations report |
|
set_clock_latency |
Defines the delay between an external clock source and the definition pin of a clock within SmartTime |
|
set_clock_uncertainty |
Specifies a clock-to-clock uncertainty and returns the ID of the created constraint if the command succeeded |
|
set_current_scenario |
Specifies the timing scenario for the Timing Analyzer to use |
|
save_design |
Writes the design to the specified filename |
|
set_defvar |
Sets the value of the Designer internal variable you specify > |
|
set_design |
Specifies the design name, family and path in which Designer will process the design |
|
set_device |
Specifies the type of device and its parameters |
|
set_disable_timing |
Disables timing arcs within a cell and returns the ID of the created constraint |
|
set_false_path |
Identifies paths that are considered false and excluded from the timing analysis in the current timing scenario |
|
set_input_delay |
Creates an input delay on a port list by defining the arrival time of an input relative to a clock in the current scenario |
|
set_max_delay |
Specifies the maximum delay for the timing paths in the current scenario |
|
set_min_delay |
Specifies the minimum delay for the timing paths in the current scenario |
|
set_multicycle_path |
Defines a path that takes multiple clock cycles in the current scenario |
|
set_output_delay |
Defines the output delay of an output relative to a clock in the current scenario |
|
smartpower_add_new_custom_mode |
Creates a new custom mode |
|
smartpower_add_new_scenario |
Creates a new scenario |
|
smartpower_add_pin_in_domain |
Adds a pin to either a Clock or Set domain |
|
smartpower_change_clock_statistics |
Changes the default frequencies and probabilities for a specific domain |
|
smartpower_change_setofpin_statistics |
Changes the default frequencies and probabilities for a specific set |
|
smartpower_commit |
Saves the changes made in SmartPower to the design file (.adb) in Designer |
|
smartpower_create_domain |
Creates a new clock or set domain |
|
smartpower_edit_custom_mode |
Edits a custom mode |
|
smartpower_edit_scenario |
Edits a scenario |
|
smartpower_initialize_clock_with_constraints |
Initializes the clock frequency and the data frequency of a single clock domain with a specified clock name and the initialization options |
|
smartpower_init_do |
Initializes the frequencies and probabilities for clocks, registers, set/reset nets, primary inputs, combinational outputs, enables and other sets of pins, and selects a mode for initialization |
|
smartpower_init_set_clocks_options |
Initializes the clock frequency of all clock domains |
|
smartpower_init_set_combinational_options |
Initializes the frequency and probability of all combinational outputs |
|
smartpower_init_set_enables_options |
Initializes the clock frequency of all enable clocks with the initialization options |
|
smartpower_init_set_othersets_options |
Initializes the frequency and probability of all other sets |
|
smartpower_init_set_primaryinputs_options |
Initializes the frequency and probability of all primary inputs |
|
smartpower_init_set_registers_options |
Initializes the frequency and probability of all register outputs |
|
smartpower_init_set_set_reset_options |
Initializes the frequency and probability of all set/reset nets |
|
smartpower_init_setofpins_values |
Initializes the frequency and probability of all sets of pins |
|
smartpower_remove_all_annotations |
Removes all initialization annotations for the specified mode |
|
smartpower_remove_custom_mode |
Removes a custom mode |
|
smartpower_remove_domain |
Removes an existing domain |
|
smartpower_remove_file |
Removes a VCD file from the specified mode |
|
smartpower_remove_pin_enable_rate |
This command is obsolete and it is replaced by smartpower_remove_pin_probability |
|
smartpower_remove_pin_frequency |
Removes the frequency of an existing pin |
|
smartpower_remove_pin_of_domain |
Removes a clock pin or a data pin from a Clock or Set domain, respectively. |
|
smartpower_remove_pin_probability |
Enables you to annotate the probability of a pin driving an enable pin |
|
smartpower_remove_scenario |
Removes a scenario from the current design |
|
smartpower_remove_vcd |
Removes an existing VCD file from a mode or entire design |
|
smartpower_restore |
Restores previously committed constraints |
|
smartpower_set_battery_capacity |
Sets the battery capacity |
|
smartpower_set_cooling |
Sets the cooling style to one of the predefined types, or a custom value |
|
smartpower_set_mode_for_analysis |
Sets the mode for cycle-accurate power analysis |
|
smartpower_set_operating_condition |
Sets the operating conditions used in SmartPower to best, typical, or worst case |
|
smartpower_set_pin_enable_rate |
This command is obsolete and it is now replaced by smartpower_set_pin_probability |
|
smartpower_set_pin_frequency |
Sets the frequency of an existing pin |
|
smartpower_set_pin_probability |
Enables you to annotate the probability of a pin driving an enable pin |
|
smartpower_set_preferences |
Sets SmartPower preferences such as power unit, frequency unit, operating mode, operating conditions, and toggle |
|
smartpower_set_scenario_for_analysis |
Sets the scenario for cycle-accurate power analysis |
|
smartpower_set_temperature_opcond |
Sets the temperature in the operating conditions used in SmartPower |
|
smartpower_set_thermalmode |
Sets the mode of computing junction temperature |
|
smartpower_set_voltage_opcond |
Sets the voltage in the operating conditions used in SmartPower |
|
smartpower_temperature_opcond_set_design_wide |
Sets the temperature for SmartPower design-wide operating conditions |
|
smartpower_temperature_opcond_set_mode_specific |
Sets the temperature for SmartPower mode-specific operating conditions |
|
smartpower_voltage_opcond_set_design_wide |
Sets the voltage settings for SmartPower design-wide operating conditions |
|
smartpower_voltage_opcond_set_mode_specific |
Sets the voltage settings for SmartPower mode-specific use operating conditions |
|
st_create_set |
Creates a set of paths to be analyzed |
|
st_commit |
Saves the changes made in SmartTime to the design (.adb) file |
|
st_edit_set |
Modifies the paths in a user set |
|
st_expand_path |
Displays expanded path information (path details) for paths |
|
st_list_paths |
Displays the list of paths in the same tabular format shown in SmartTime |
|
st_remove_set |
Deletes a user set from the design |
|
st_restore |
Restores constraints previously committed in SmartTime |
|
st_set_options |
Sets options for timing analysis |
|
timer_add_clock_exception |
Adds an exception to or from a pin with respect to a specified clock |
|
timer_add_pass |
Adds the pin to the list of pins for which the path must be shown passing through in the timer |
|
timer_add_stop |
Adds the specified pin to the list of pins through which the paths will not be displayed in the timer |
|
timer_commit |
Saves the changes made to constraints in Timer into the Designer database. |
|
timer_get_path |
Displays the Timer path information in the Log window |
|
timer_get_clock_actuals |
Displays the actual clock frequency in the Log window |
|
timer_get_clock_constraints |
Displays the clock constraints (period/frequency and dutycycle) in the Log window |
|
timer_get_maxdelay |
Displays the maximum delay constraint between two pins of a path in the Log window |
|
timer_get_path_constraints |
Displays the path constraints set for maxdelay in the Timer in the Log window |
|
timer_remove_clock_exception |
Removes the previously set clock constraint |
|
timer_remove_pass |
Removes the previously entered path pass constraint |
|
timer_remove_stop |
Removes the path stop constraint on the specified pin |
|
timer_restore |
Restores previously committed constraints |
|
timer_setenv_clock_freq |
Sets a required clock frequency, in MHz, for the specified clock |
|
timer_setenv_clock_period |
Sets the clock period constraint for the specified clock |
|
timer_set_maxdelay |
Adds a maximum delay constraint for the path |
|
timer_remove_all_constraints |
Removes all the timing constraints previously entered in the Designer system |