13.33.203 timer_get_maxdelay
Displays the maximum delay constraint between two pins in a path in the Log window.
timer_get_maxdelay -from source_pin -to destination_pin
Arguments
-from source_pin
Specifies the name of the source pin in the path.
-to destination_pin
Specifies the name of the destination pin in the path.