13.33.145 smartpower_add_new_custom_mode

Creates a new custom mode.

smartpower_add_new_custom_mode -name {mode_name} -base_mode {base_mode} -description {mode_description}

Arguments

-name {mode_name}

Specifies the name of the new custom mode.

-base_mode {base_mode}

Specifies the name of the base mode used to create the new custom mode.

-description {mode_description}

Specifies the description of the new custom mode.