13.33.157 smartpower_init_setofpins_values

Initializes the frequency and probability of all sets of pins.

smartpower_init_setofpins_values -domain_name {name} -freq {value} -proba {value}

Arguments

-domain_name{name}

Specifies the set of pins that will be initialized. The following table shows the acceptable values for this argument:

ValueDescription

IOsEnableSet

Specifies that the IOsEnableSet set of pins will be initialized

MemoriesEnableSet

Specifies that the MemoriesEnableSet set of pins will be initialized

-freq {value}

Specifies the user input frequency in Hz, MHz, or KHz.

-proba {value}

Specifies the user input probability in %.