13.33.130.5.1 Arguments
filename
Specifies the name and destination of the timing report.
-type timing
Specifies the type of report to generate.
−print_summary value
Specifies whether to print the summary section in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes summary section in the timing report (the default value). |
|
no |
Excludes summary section in the timing report |
−analysis value
Specifies whether the report will consider minimum analysis or maximum analysis.
| Value | Description |
|---|---|
|
min |
Timing report considers minimum analysis |
|
max |
Timing report considers maximum analysis (the default value) |
−use_slack_threshold value
Specifies whether the report will consider slack threshold.
| Value | Description |
|---|---|
|
yes |
Includes slack threshold in the timing report. |
|
no |
Excludes slack threshold in the timing report (the default value) |
−slack_threshold value
Specifies the threshold to consider when reporting path slacks. This is a floating-point number in nanoseconds (ns). By default, there is no threshold (all slacks are reported).
−print_paths value
Specifies whether the path section (clock domains and in-to-out paths) will be printed in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes path section in the timing report (the default value) |
|
no |
Excludes path sections from the timing report |
−max_paths value
Defines the maximum number of paths to display for each set. This is a positive integer value greater than zero. The default is 5.
−max_expanded_paths value
Defines the number of paths to expand per set. This is a positive integer value greater than zero. The default is 1.
−include_user_sets value
Defines whether to include the user defined sets in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes user defined sets in the timing report (the default value) |
|
no |
Excludes user defined sets from the timing report |
−include_pin_to_pin value
Specifies whether to show pin-to-pin paths in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes pin-to-pin paths in the timing report (the default value). |
|
no |
Excludes pin-to-pin paths from the timing report |
−include_clock_domains value
Defines whether to include clock domains in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes clock domains |
|
no |
Excludes clock domains from the timing report |
−select_clock_domains value
Specifies whether to show the clock domain list in the timing report.
| Value | Description |
|---|---|
|
yes |
Includes the clock domain list in the timing report |
|
no |
Excludes the clock domain list from the timing report (the default value) |
−clock_domain clock_domain_list
Defines the clock domain to be considered in the clock domain section. The domain list is a series of strings with domain names separated by spaces. Both the summary and the path sections in the timing report display only the listed clock domains.
−format value
Specifies the output format of the generated the report.
| Value | Description |
|---|---|
|
text |
Generates a text report; text is the default value |
|
csv |
Generates the report in a comma-separated value format which you can import into a spreadsheet |