13.33.83.1 Arguments

-placer_high_effort value

The following table shows the acceptable values for this argument:
ValueDescription

off

Disables physical synthesis of combinational logic. This is the default.

on

Enables physical synthesis of combinational logic

-seq_opt value

The following table shows the acceptable values for this argument:
ValueDescription

off

Disables physical synthesis of sequential logic. This is the default.

on

Enables physical synthesis of sequential logic in high-effort mode

-mindel_repair value

The following table shows the acceptable values for this argument:
ValueDescription

off

Does not run minimum delay violations repair. This is the default.

on

Enables repair of minimum delay violations during route

-placer_seed value

An integer value that you can set to change the initial random seed number for the placement.

-show_placer_seed value

Causes Layout to display the initial random seed number used for the placement.