13.33.124.2 Description
Removes a maximum delay value from the specified clock in the current scenario. If the arguments do not match a maximum delay constraint in the current scenario, or if the specified ID does not refer to a maximum delay constraint, this command fails.
Do not specify both the maximum delay arguments and the constraint ID.