13.33.122.2 Description
Removes an input delay from the specified clocks and port in the current scenario. If the clocks and port names do not match an input delay constraint in the current scenario, or if the specified ID does not refer to an input delay constraint, this command fails.
Do not specify both the clock and port names and the constraint ID.