13.33.120.2 Description
Removes a false path from the specified clock in the current scenario. If the arguments do not match a false path constraint in the current scenario, or if the specified ID does not refer to a false path constraint, this command fails.
Do not specify both the false path arguments and the constraint ID.