13.33.91.1 Arguments
-extended_run value
The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
|
off |
Skips extended run mode. This is the default. |
|
on |
Invokes extended run mode |
-placer_seed value
An integer value that you can set to change the initial random seed number for the placement.
-show_placer_seed
Causes Layout to display the initial random seed number used for the placement.