13.33.4.1 add_profile

Sets the same values as the Add or Edit Profile dialog box.

add_profile -name profilename -type value -tool profiletool -location tool_location [-args

tool_parameters] [-batch value]

Arguments

-name profilename

Specifies the name of your new profile.

-type value

Specifies your profile type, where value is one of the following:

Table 13-34. Values
ValueDescription

synthesis

New profile for a synthesis tool

simulation

New profile for a simulation tool

stimulus

New profile for a stimulus tool

flashpro

New FlashPro tool profile

coreconfig

New CoreConsole tool profile

-tool profiletool

Name of the tool you are adding to the profile.

-location tool_location

Full pathname to the location of the tool you are adding to the profile.

-args tool_parameters

Profile parameters (if any).

-batch value

Runs the tool in batch mode (if TRUE). Possible values are:

ValueDescription

TRUE

Runs the profile in batch mode

FALSE

Does not run the profile in batch mode