13.33.69.3.46 Example

The following code will determine if a design has been modified.

set bDesignModified [ is_design_modified ] if { $bDesignModified == 0 } {

puts “Design has not been modified.”

}

See Also get_design_filename get_design_info is_design_loaded is_design_state_complete

is_design_state_complete

is_design_state_complete value

Returns a Boolean value (0 for false, 1 for true) indicating if a specific design state is valid. True is returned if the specified design state is valid.