13.33.69.3.9 Arguments

-attribute{value}

This specifies the attribute for which the values will be applied. The following table shows the acceptable values for this argument:

Value

Description

outdrive

Applies suggested outdrive values

slew

Applies suggested slew values

-io {value}

This selects the I/Os for which the suggestion will be applied. To select multiple I/Os, use -io {value} for each I/O.