13.33.69.3.50 Exceptions

  • The command will return an error if a design is not loaded.
  • The command will return an error if more than one argument is passed.
  • The command will return an error if the argument is not one of the valid values.