13.33.69.3.41 Example

The following code will determine if a design has been loaded.

set bDesignLoaded [ is_design_loaded ] if { $bDesignLoaded == 0 } {

puts “No design is loaded.”

}

See Also get_design_filename get_design_info is_design_modified is_design_state_complete

is_design_modified

is_design_modified

Returns a Boolean value (0 for false, 1 for true) indicating if a design has been modified in the Designer software. True is returned if a design has been modified.