5.34.130.14 Arguments
uncertainty
Specifies the time in nanoseconds that represents the amount of variation between two clock edges.
-from
Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the source clock list. Only one of the -from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
-rise_from
Specifies that the clock-to-clock uncertainty applies only to rising edges of the source clock list. Only one of the - from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
-fall_from
Specifies that the clock-to-clock uncertainty applies only to falling edges of the source clock list. Only one of the - from, -rise_from, or -fall_from arguments can be specified for the constraint to be valid.
from_clock_list
Specifies the list of clock names as the uncertainty source.
-to
Specifies that the clock-to-clock uncertainty applies to both rising and falling edges of the destination clock list. Only one of the -to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
-rise_to
Specifies that the clock-to-clock uncertainty applies only to rising edges of the destination clock list. Only one of the
-to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
-fall_to
Specifies that the clock-to-clock uncertainty applies only to falling edges of the destination clock list. Only one of the -to, -rise_to , or -fall_to arguments can be specified for the constraint to be valid.
to_clock_list
Specifies the list of clock names as the uncertainty destination.
-setup
Specifies that the uncertainty applies only to setup checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks.
-hold
Specifies that the uncertainty applies only to hold checks. If none or both -setup and -hold are present, the uncertainty applies to both setup and hold checks.