5.34.130.229 Arguments
-powerunit {value}
Specifies the unit in which power is set. The following table shows the acceptable values for this argument:
Value | Description |
W | The power unit is set to watts |
mW | The power unit is set to milliwatts |
uW | The power unit is set to microwatts |
-frequnit {value}
Specifies the unit in which frequency is set. The following table shows the acceptable values for this argument:
Value | Description |
Hz | The frequency unit is set to hertz |
kHz | The frequency unit is set to kilohertz |
MHz | The frequency unit is set to megahertz |
-opmode {value}
Specifies the operating mode. The following table shows the acceptable values for this argument:
Value | Description |
active | The operating mode is set to active |
static | The operating mode is set to static |
sleep | The operating mode is set to sleep |
Flash*Freeze | The operating mode is set to Flash*Freeze |
shutdown | The operating mode is set to shutdown |
-opcond {value}
Specifies the operating condition. The following table shows the acceptable values for this argument:
Value | Description |
worst | The operating condition is set to worst case |
typical | The operating condition is set to typical case |
best | The operating condition is set to best case |
-toggle {value}
Specifies the toggle. The following table shows the acceptable values for this argument:
Value | Description |
true | The toggle is set to true |
false | The toggle is set to false |