5.34.130.244 Arguments
-mode {value}
Specifies the mode in which the junction temperature is computed. The following table shows the acceptable values for this argument:
Value | Description |
ambient | The junction temperature will be iteratively computed with total static power |
opcond | The junction temperature will be given as one of the operating condition range values specified in the device selection |