5.34.130.282 Arguments

-name name

Specifies the name of the set to modify.

-source pin_list

If the set is a subset of another set, specifies a filter on the source pins from the parent set. Otherwise, this option specifies the source pins of the set.

-sink pin_list

If the set is a subset of another set, specifies a filter on the sink pins from the parent set. Otherwise, this option specifies the sink pins of the set.

-rename_to name

Specifies a new name for the set.