5.34.130.204 Arguments

-style {value}

Specifies the cooling style to custom value or to one of the predefined types with a default thermal resistance value. The following table shows the acceptable values for this argument:

Value

Description

300_lfm

Predefined cooling style

case_cooling

Predefined cooling style

still_air

Predefined cooling style

custom

Cooling style defined by user input

-teta {value}

Specifies the thermal resistance in °C/W. This argument is only available when style is set to Custom.