5.34.130.223 Examples
The following example sets the probability of the pin driving the enable pin of a bidirectional I/O
smartpower_set_pin_enable_rate -pin_name mybibuf/U0/U1:EOUT \ –pin_enable_rate 50.4
smartpower_set_pin_frequency
smartpower_set_pin_frequency -pin_name {pin_name} -pin_freq {value}
Sets the frequency of a pin in megahertz (MHz). If you do not use this command, each pin will have default frequency based on its domain.