5.34.130.370 Arguments
-from source_pin
Specifies the name of the source pin in the path.
-to destination_pin
Specifies the name of the destination pin in the path.
-unit {value}
Specifies whether the delay unit is in nanoseconds or picoseconds. The following table shows the acceptable values for this argument:
Value | Description |
ns | Sets the delay in nanoseconds |
ps | Sets the delay in picoseconds |
-delay delay_value
Specifies the actual delay value for the path.