5.34.130.203 Examples
The following example sets the battery capacity to 40 A/h:
smartpower_set_battery_capacity {40}
smartpower_set_cooling
Sets the cooling style to one of the predefined types, or a custom value.
smartpower_set_cooling -style {value} -teta {value}