5.34.130.192 Arguments
-from {value}
This specifies the if the VCD is removed for a specific mode or for the entire project. The following table shows the acceptable values for this argument:
Value | Description |
mode | The VCD file is removed for a mode |
project | The VCD file is removed from the project |
-mode {value}
This specifies the name of the mode for which the VCD will be removed
-filename
This specifies the name of the VCD file to be removed