5.34.130.290 Arguments
-set name
Displays a list of paths from the named set. You can either use the –set option to specify a set name, or use both – clock and –type to specify a set. A list of valid set names includes “in_to_out”, as well as any user set names.
-clock clock_id
Displays the set of paths belonging to the specified clock domain. You can either use this option along with -type to specify a set or use the -set option to specify the name of the set to display.
-in_to_out
Specifies that the paths should be from the set “Input to Output”, which includes paths that start at input ports and end at output ports.
-type value
Specifies the type of paths in the clock domain to display in a list. You can only use this option with the -clock option, not by itself. You can either use this option along with -clock to specify a set or use the -set option to specify a set name.
Value | Description |
reg_to_reg | Paths between registers in the design |
async_to_reg | Paths from asynchronous pins to registers |
reg_to_asyn | Paths from registers to asynchronous pins |
external_recovery | The set of paths from inputs to asynchronous pins |
external_removal | The set of paths from inputs to asynchronous pins |
external_setup | Paths from input ports to registers |
Paths from input ports to registers | |
clock_to_out | Paths from registers to output ports |
-source_clock clock_id
Displays a list of timing paths for an inter-clock domain set belonging to the source clock specified. You can only use this option with the -sink_clock option, not by itself.
-sink_clock clock_id
Displays a list of timing paths for an inter-clock domain set belonging to the sink clock specified. You can only use this option with the -source_clock option, not by itself.
-source pin_list
Specifies a filter on the source pins of the paths to be listed.
-sink pin_list
Specifies a filter on the sink pins of the paths to be listed.
-analysis name
Specifies the analysis type for the paths to be listed. The following table shows the acceptable values for this argument:
Value | Description |
maxdelay | Maximum delay analysis |
mindelay | Minimum delay analysis |
-format value
Specifies the file format of the output. The following table shows the acceptable values for this argument:
Value | Description |
text | ASCII text format |
csv | Comma separated value fie format |