5.34.130.286 Arguments

-set name

Displays a list of paths from the named set. You can either use the -set option to specify a set name, or use both - clock and -type to specify a set. A list of valid set names includes "in_to_out", as well as any user set names.

-clock clock_id

Displays the set of paths belonging to the specified clock domain. You can either use this option along with -type to specify a set or use the -set option to specify the name of the set to display.

-in_to_out

Specifies that the paths should be from the set "Input to Output, which includes paths that start at input ports and end at output ports.

-type value

Specifies the type of paths in the clock domain to display in a list. You can only use this option with the -clock option, not by itself. You can either use this option along with -clock to specify a set or use the -set option to specify a set name.

Value

Description

reg_to_reg

Paths between registers in the design

async_to_reg

Paths from asynchronous pins to registers

reg_to_asyn

Paths from registers to asynchronous pins

external_recovery

The set of paths from inputs to asynchronous pins

external_removal

The set of paths from inputs to asynchronous pins

external_setup

Paths from input ports to registers

Paths from input ports to registers

clock_to_out

Paths from registers to output ports

-source_clock clock_id

Displays a list of timing paths for an inter-clock domain set belonging to the source clock specified. You can only use this option with the -sink_clock option, not by itself.

-sink_clock clock_id

Displays a list of timing paths for an inter-clock domain set belonging to the sink clock specified. You can only use this option with the -source_clock option, not by itself.

-source pin_list

Specifies a filter on the source pins of the paths to be listed.

-sink pin_list

Specifies a filter on the sink pins of the paths to be listed.

-analysis name

Specifies the analysis type for the paths to be listed. The following table shows the acceptable values for this argument:

Value

Description

Value

Description

maxdelay

Maximum delay analysis

mindelay

Minimum delay analysis

-index list_of_indices

Specifies which paths to display. The index starts at 1 and defaults to 1. Only values lower than the max_paths option will be expanded.

-format value

Specifies the file format of the output. The following table shows the acceptable values for this argument:

Value

Description

text

ASCII text format

csv

Comma separated value fie format