5.34.130.21 Description
A timing scenario is a set of timing constraints used with a design. If the specified scenario is already the current one, this command has no effect.
After setting the current scenario, constraints can be listed, added, or removed, the checker can be invoked on the set of constraints, and so on.
This command uses the specified timing scenario to compute timing analysis.