21.5.99 MSS External Status Register
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:19] | Reserved | 0 | |
| 18 | CC_HRESP_ERR | Indicates whether any accesses to the corresponding master on the CACHE resulted in HRESP assertion by the slave to the CACHE (and hence to the master) or HRESP generated by the CACHE itself to the master (in the case of an invalid address being accessed). The CACHE does pass the HRESP signal through to the requesting master, but the event is also registered in this register. The bit definitions are as follows: Bit 0: Corresponds to an HRESP assertion being issued to the DCode bus master. Bit 1: Corresponds to an HRESP assertion being issued to the ICode bus master. Bit 2: Corresponds to an HRESP assertion being issued to the SBus master. | |
| 17 | DDRB_LOCK_MID | 0 | Indicates which master (AHB bus or HPDMA) is responsible for lock timeout condition. 0: AHB bus master 1: HPDMA |
| 16 | DDRB_LCKOUT | 0 | Asserted when lock timeout counter reaches its maximum value. Lock time out counter (20-bit) is maintained in the MSS DDR bridge, which starts counting when a locked transfer obtains access to the AXI bus. When the counter reaches maximum value, a DDRB_LCKOUT interrupt is generated and stays asserted until cleared by the processor. |
| 15 | DDRB_HPD_WR_ERR | 0 | Asserted when the MSS DDR bridge gets an error response from the DDR slave for an HPDMA write request. Address of write transaction for which error response is received is provided by DDRB_HPD_ERR_ADD. |
| 14 | DDRB_SW_WR_ERR | 0 | Asserted when the MSS DDR bridge gets an error response from the DDR slave for an AHB bus master write request. Address of write transaction for which error response is received is provided by DDRB_SW_ERR_ADD. |
| 13 | DDRB_DS_WR_ERR | 0 | Asserted when the MSS DDR bridge gets an error response from the DDR slave for a DS master write request. Address of write transaction for which error response is received is provided by DDRB_DS_ERR_ADD. |
| [12:7] | DDRB_RDWR_ERR_REG | 0 | Provides the read/write address match error status generated during the following accesses: Bit 0 = 1: AHB bus and HPDMA are trying to access same address Bit 1 = 1: AHB bus and DS are trying to access same address Bit 2 = 1: HPDMA and DS are trying to access same address Bit 3 = 1: IDC and HPDMA are trying to access same address Bit 4 = 1: IDC and AHB Bus are trying to access same address Bit 5 = 1: IDC and DS are trying to access same address |
| [6:0] | SW_ERRORSTATUS | 0 | Indicates whether any accesses by the corresponding master on the AHB bus resulted in either HRESP assertion by the slave to the AHB bus, HRESP assertion by the AHB bus to that master (in the case of blocked fabric master), or was decoded by the AHB bus as being to “unimplemented” address space. The bit definitions are as follows: Bit 0: Corresponds to an HRESP assertion being issued to the HPDMA interface Bit 1: Corresponds to an HRESP assertion being issued to FIC_0 interface Bit 2: Corresponds to an HRESP assertion being issued to FIC_1 System interface S interface Bit 3: Corresponds to an HRESP assertion being issued to the Ethernet MAC Bit 4: Corresponds to an HRESP assertion being issued to the peripheral DMA engine Bit 5: Corresponds to an HRESP assertion being issued to the USB Bit 6: Corresponds to an HRESP assertion being issued to the System Controller These signals are not used as interrupts to the Cortex-M3 processor. Instead, they are ORed together in SYSREG to create a signal called SW_ERRORINTERRUPT, which is used as an interrupt to the Cortex-M3 processor. |