21.5.39 MSS DDR Fabric Alignment Clock Controller Configuration Register 2

Table 21-47. MSSDDR_FACC2_CR
Bit NumberNameReset ValueDescription
[31:14]Reserved0—
13MSS_XTAL_RTC_EN0x1Enable signal for auxiliary crystal oscillator (RTC crystal oscillator)
12MSS_XTAL_EN0x1Enables the signal for the main crystal oscillator. If the main crystal oscillator is selected as the MSS Flash*Freeze clock source, this bit must be asserted at all times (even when not in Flash*Freeze mode).

1: Enable

0: Disable

11MSS_CLK_ENVM_EN0x1Enables internal eNVM RC oscillator. Configure this field statically. Do not write to this field while the source clock is active.
10MSS_1MHZ_EN0x1Enables the signal for the 1 MHz RC oscillator. If the 1 MHz RC oscillator is selected as the MSS Flash*Freeze clock source, this bit must be asserted at all times (even when not in Flash*Freeze mode).

1: Enable

0: Disable

9MSS_25_50MHZ_EN0x1Enables the signal for the 50 MHz RC oscillator. If the 50 MHz RC oscillator is selected as the MSS Flash*Freeze clock source, this bit must be asserted at all times (even when not in Flash*Freeze mode).

1: Enable

0: Disable

[8:6]FACC_STANDBY_SEL0Contains the select lines for the three 2 to 1 no-glitch multiplexers, which implement the 4 to 1 no-glitch standby MUX function. This is used to allow one of four possible clocks to proceed through to the MSS during FACC PLL Initialization Time. There are two MUXes in the first rank, and these feed into a third MUX in the second rank.

Bit 6 feeds into one of the first rank 2 to 1 MUXes (Standby MUX 0) and is defined as follows:

0: MUX 0 output comes from RCOSC_25_50MHZ

1: MUX 0 output comes from XTLOSC_CLK

Bit 7 feeds into one of the first rank 2 to 1 MUXes (Standby MUX 1). Bit 7 must always be 0 and defined as follows:

0: MUX 1 output comes from RCOSC_1MHZ

Bit 8 feeds into the second rank 2 to 1 MUX (Standby MUX 2) and is defined as follows:

0: MUX 2 output comes from MUX 0

1: MUX 2 output comes from MUX 1

Do not write to this field while the standby clock is active.

5FACC_PRE_SRC_SEL0Must always be 0, and defined as follows:

0: RCOSC_1MHZ is fed through to the source no-glitch clock multiplexer.

[4:2]FACC_SRC_SEL0Contains the select lines for the three 2 to 1 no-glitch multiplexers, which implement a 4 to 1 no-glitch source MUX function. There are two MUXes in the first rank, and these feed into a third MUX in the second rank.

Bit 2 feeds into one of the first rank 2 to 1 MUXes (Source MUX 0) and is defined as follows:

0: MUX 0 output comes from RCOSC_25_50MHZ

1: MUX 0 output comes from XTLOSC_CLK

Bit 3 feeds into one of the first rank 2 to 1 MUXes (Source MUX 1) and is defined as follows:

0: MUX 1 output comes from RCOSC_1MHZ

1: MUX 1 output comes from MPLL_OUT_CLK

Bit 4 feeds into the second rank 2 to 1 MUX (Source MUX 2) and is defined as follows:

0: MUX 2 output comes from MUX 0

1: MUX 2 output comes from MUX 1

When switching any of the no-glitch MUXes, both the clock being switched from and the clock being switched to must be running. Do not write to this field while the source clock is active.

[1:0]RTC_CLK_SEL0Indicates which of the possible clocks are to be configured as the source of the MSS RTC clock. The allowed values are as follows:

00: RTC_CLK comes from XTLOSC_CLK

01: RTC_CLK comes from RCOSC_1MHZ

10: RTC_CLK comes from RCOSC_25_50MHZ

11: RTC_CLK comes from RTC_XTLOSC_CLK

The reset signal for this bit is SYSRESET_N.